Contacts and coils
| Contacts | Coils |
|---|---|
| Normally Open -| |- | Energize -( )- |
| Normally Closed -|/|- | De-energize -(/)- |
| Positive Transition -|P|- | Set (LatchThe control word is used to activate the drive's latch status machine. The latch control word is processed independently of the EtherCAT bus cycle. The status word is used to return the drive's latch status) -(S)- |
| Negative Transition -|N|- | Reset (Unlatch) -(R)- |
| Normally closed positive transition -|/P|- | Positive transition sensing coil -(P)- |
| Normally closed negative transition -|/N|- | Negative transition sensing coil -(N)- |
|
Copyright © 2018 Kollmorgen |
|